付属品無成分【有効成分】メトフルトリン540mg/本【その他の成分】1号灯油、流動パラフィン、香料使用方法(1)ボトルのキャップを回し、キャップが芯に触れないようにゆっくり真上に引き抜いてください。芯は折れることがありますので、ていねいにお取り扱いください。※キャップは捨てずに保管しておいてください。ボトルを保管する際に必要です。(2)器具(下)の三角印をLOCKからOPENにスライドさせ、器具(上)をまっすぐ持ち上げてください。(3)ボトルを器具(上)の下方よりカチッと音がするまで確実に差し込んでセットしてください。その際、器具上部の蒸散口の中を見て、黒色の芯がリングヒーター(銀色)に触れないようにしてください。(4)器具(下)を下方より確実に押し込んでください。(5)器具(下)の三角印をOPENからLOCKにスライドさせてください。(6)プラグをコンセント(家庭用100Vの電源)に差し込みスイッチを入れてください。しばらくすると成分が部屋中に揮散し始めます。※電源コードに重いものを載せたり、機器にはさまないでください。(7)※蒸散口のある方が器具(上)です。上下逆に使用すると液漏れ等の可能性がありますのでご注意ください。【取替え方法】ボトルを必ず下にしてまっすぐ下方に引っぱってください。はずしにくいときは、スイッチを入れて30分ほど器具を温めてからはずしてください。液残量が「おとりかえライン」になったら、新しいボトルをご用意ください。【ご使用の器具の点検を!】●電源コード:電源コードにキズ、亀裂等があったり、コードを動かすとランプが消灯する器具は、感電や発火の原因となり危険です。直ちにご使用を中止し、新しい器具をお買い求めください。※蒸散口の上に遮蔽物があったり、横に寝かせて使用するなどして、コードに薬液が付着するとコードが硬くなり劣化が進むことがあります。※電源コードは交換することができません。コードが破損した場合は、器具を廃棄してください。器具を長年(7年から8年)使用すると経年劣化を起こす可能性が高くなります。使用方法や使用環境によっては劣化が早くなることもあります。安全にご使用いただくため、新しい器具をお買い求めください。●蒸散口:使用方法や使用環境によっては蒸散口が劣化し、破損しやすくなる可能性があります。蒸散口が破損した場合は、やけどの恐れがあるので絶対に指などを入れないでください。直ちにご使用を中止し、新しい器具をお買い求めください。香り無香性対象害虫ゴキブリ医薬品医療機器等法防除用医薬部外品FSC認証認定FSC認証番号C131331販売名アース虫ケアHAT2-2