Electrodynamic Exciter Drivers
Visaton Exciters are designed to convert a flat panel into a loudspeaker instead of fitting a conventional loudspeaker
Panels of many different materials and sizes can be used such as plywood, polystyrene ceiling tiles and plexiglass
Exciters provide an invisible sound source which is also proof against external influences (water, dust, sharp objects)
Sound quality can be very good and their non directional sound production means that positioning in a room is not so important as with conventional speakers
Exciters are easy to install and do not require holes cutting to accommodate them
Exciters are a new and innovative type of speaker
They are electromagnetic devices which connect to an ordinary audio amplifier in the conventional way by means of loudspeaker cable
Once fixed in place to the rear of a panel, the audio signal causes the exciter unit to vibrate which in turn makes the panel to which it is fixed vibrate and create sound
The quality of the reproduced sound is very much dependent on the type of surface the exciter is attached to
The sound will generally be better with larger panels which are light and rigid
Measurements such as frequency response and sound pressure level will depend on the surface material
Ideally the exciter should be fitted slightly off centre on the panel and should be firmly attached by means of gluing and/or screwing.
仕様●インピーダンス:8Ω●ドライバーの形状:長方形●スピーカードライバーサイズ:8 cm (3 in) 以下●長さ:46mm●幅:46mm●奥行き(深さ):17mm●重さ:60g●RoHS適合状況:適合●コード番号:719-1954アズワン品番68-4150-45
Visaton K 16 シリーズは、プラスチックバスケットとプラスチック製ダイアフラムを備えたミニチュアスピーカーです。プラスチック製で、ABS (バスケット)を備えています UL 94 HB Mylarダイアフラムこのスピーカーは、耐候性と耐紫外線性を備えています。広範な周波数応答により、優れた音声再生を実現します。屋外用途や大気条件が一般的に好ましくない
仕様●コイル抵抗:16Ω●サウンドレベル:84dB●定格出力:2W●コーン材質:マイラー●寸法:50 (Dia.) x 18mm●直径:50mm●高さ:18mmアズワン品番65-7097-20